This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2116: ON-Resistance of TPS2116 when Iout=1A

Part Number: TPS2116

Hi team,

Customer wants to know the On-Resistance when the Iout=1A.

Can you share the TYP and MAX of the On-Resistance when Iout=1A as in the Datasheet?

Best regards,

Foong Wei Seng

  • Foong,

    We do not have this data to provide, however checking with the backend team it appears that the actual load current is not going to have an impact on the ON resistance. The load current would attribute to heat, however as we already spec the ON resistance across different temperature ranges you can just use the relevant on resistance for 1A even though the test condition is 200mA.

    Best Regards,
    Tim