Other Parts Discussed in Thread: LP8556, TPS65132
Hello,
We have a problem in LM36274 debugging.
The LM36274 can work well when PWM disabled.
But the LM36274 does not work when the 75HZ PWM signal is input.
So we would like to ask how to set all the registers of LM36274 when the PWM signal below is input.
Input PWM signal waveform:

Schematic: input voltage is 5V
load infromation :VF is 21V ; ILED is 43mA(@75HZ, 10%duty)