Dear TI experts,
We encountered a problem when using LP877451. After PCBA was powered on, there was an instantaneous voltage pulse below 3V at the input end of LP877451, and then the input end remained stable at 3.28V.
Enable was also at a high level of 3.23V, and the measured VOUT LDO was 1.8V.
However, nRSTOUT remained low and there were no outputs in several channels.
Please help to see what the problem is,
To exit this state, can I only power on or reset the LP877451 again. Is this the characteristic of LP877451?
Thanks.