Hi team,
As shown in the figure is the description of the EEPROM chapter of LP8860. What is the logical relationship between 00h~1Ah and 60h~78h? For example: The customer sets the current value of each channel. 0x60, 0x61, 0x02, and 0x03 are all registers for configuring the current of each channel. During the configuration process, we found that only by changing the 0x02 and 0x03 registers can we get the current we want.