Hello,
I had previously opened a ticket regarding the LM5176, where we had issues with no output voltage, chips heating up, etc.
We redid some of the design, and produced new PCB's. We assembled them, with the same behavior on the boards.
We then proceded to assemble a new PCB, but with all the components from your Evaluation Board LM5176EVM-HP.
Right after assembling this board, during testing, the LM5176 did not heat up, the output voltage was pretty much ok (we were expecting 12V, the voltage was around 12.5V which is ok), and we increased the Load Value up to 1.5A without any issue whatsoever. We had the load at the 1.5A mark for around 5 to 10 minutes, when suddenly, the output voltage dropped to ~9V, and no power could be delivered. Without load, the voltage would stay at 9V, but even with a very small load of 100mA, the output voltage dropped to 0V.
After this, the IC started heating up again, this time less than before, but there is a fixed consumption of about 50m.
In the last response on my last ticket https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1236935/lm5176-output-voltage-too-low-ic-heating-up-fast/4782936, by Stefan Schauer, the most visible issue was with the VCC line, which is now ok, at around 7V.
My main issues right now are 2 things:
1. Why does this PCB work fine (at least for 10 minutes) with the component values from your Evaluation Boards, but does not work with the component values from your Webench Power Designer? Can the designer provide wrong values?
2. Why does the chip suddently die after 10 minutes, with a fixed & stable power supply, and also a fixed and stable DC electronic load. There were no voltage spikes, no current spikes, and still the chip is not working!
Best regards,
Carlos Mesquita