hi Team,
what if a customer were to permanently operate TLV71333PDBVR above recommended Vin 5.5V, but below abs max of 6.5V? Would it reduce lifetime? Could you estimate by how much? Other effects?
Regards
Andreas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andreas,
How far above 5.5V would they be operating? The lifetime would probably degrade somewhat depending on how close to the 6.5V abs max limit they operate, but estimating the extent of the degradation is not trivial so I cannot give you a number.
Regards,
Nick
Yes, sorry, you are right, the abs max is 6V. The question is concerning an existing design with max Vin of 5.781. Can you help with an assessment of what that could mean for the LDO in the long run?
Regards
Andreas
Hi Andreas,
I talked to design and it is not easy to estimate the risk level for this device because the technology process that is used does not support FIT rate estimations through simulations, so the only way would be through qual which is a much bigger ask.
Regards,
Nick