Hi,
I have a question concerning how to interpret the datasheet for the VCn voltages.
I have designed a circuit that should be able to handle both 6S and 12S depending on which resistors you mount. For 6S we connect VC7 and up to the BAT-pin as described in the datasheet. This worked well and we got everything to run as expected. Then we tried to apply 12S (48V) without modifying the resistors and that killed the IC. We also did not have any cell voltages connected, just powering the VBAT-pin.
We interpreted the datasheet so that it would not be any problem to connect it this way. So my main question is if this was wrongly interpreted or if we have another problem that caused this issue.
Best Regards, Jimmy