I encounter three problems when I use tps563201.
1.When DCM mode,switch node have overshoot voltage.Why? Which parameter should I adjust.

2.When CCM mode,switch node have undershoot voltage.Why? Which parameter should I adjust.

3.Output Voltage Vary with load,when load is 1A,output is 3.34V,when load is 2A,output is 3.29V,when load is 3A,output is 3.23V,Why? Which parameter should I adjust.
Our schematic is as below,thanks!