Hi team,
My customer faced a simulation problem, about the invalid reverse polarity protection function. The simulation files are attached following:
TPS12110-Q1_PSPICE_TRANS_X-2023-11-20-[09.15.18].rar
Here provides some problem description during the simulation, and they are all based on the provided simulation file.
- The simulation is based on the grounded INP pin.
- In order to simulate the reverse voltage, a -30V voltage source is launched at 250mV.
- SRC pin is pulled low. However, PD/PU has not been pulled low following. There is a voltage difference between GS, and the MOS is conducted.
- What's more, when performing short-circuit protection shutdown simulation, PD/PU is limited at 0V, without following SRC, too.
Pls help review the simulation file, and find out why the reverse voltage problem function is valid in this case.
Thanks a lot.
Best regards,
Matt.