Dear experts:
I have read SLLU237A.pdf - HD3SS3220 DFP Dongle Evaluation Module. In Figure 3. Capacitor Placement, 0.47uF (470nF) AC coupling capacitors are selected in the schematics. According to USB 3.2 V1.2 specification (the latest version), the AC decoupling capacitors on RX side should be between 297nF and 363nF (please see Table 6-22 Receiver Normative Electrical Parameters).
This issue also can be found in the EVB boards of other vendors sometimes. ITE USB switch IT5205 even uses 0.68uF in the reference schematics.
I am trying to get the answer of this issue.
By the way, I found an ECN (20131608-ECN) on TI E2E forum by accident (the link information shows, it's from TI E2E forum). But it seems not be a formal ECN from USB-IF.
Best regards.
Charles Lai