I'm working in offline mode for Power Designer. I noticed that after changing the output caps in the schematic editor and clicking "OK", the Bode plot automatically updates, but the time domain transient plots do not. I can get those plots to update if I first switch over to another output rail and then switch back. That trick seems to force the screen to update.The notes that pop up when I hit the "Apply & Recalculate" button claim that the "OK" button automatically recalculates the design, but I'm not seeing that happen (except for the small-signal plots).
I've been experiencing another strange problem with the schematic editor where it forgets (or doesn't save) my changes to the output caps if I do it at the same time as changing the output inductor. In the schematic editor, I have the following boxes unchecked: "Select inductor" and "Select capacitor legs based on # phases". I can get it to recognize both inductor and cap changes by first changing the inductor and clicking "OK". Then I open the schematic editor back up and change the caps. But, if I do them both at the same time and check "OK", it reverts my capacitor changes back to what it was before my change.