Other Parts Discussed in Thread: TPS63900, , TPSM83100, TPS631000
Can we put on the input side of the TPS63900EVM a battery pack with HLC with a voltage level between 2.7 and 3.6 volts. And on the output side can we make a voltage of 3V3 with a load of 600mA (or what could the TPS63900 deliver in mA under these conditions? Temperature environment can vary from -20 to +75 degrees celcius.
And if the TPS63900 is not suitable is there any other solution available?