This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27402: Problem with adding constant current limit

Part Number: LM27402


Hi Team,

I have some LM27402 module on hand, which works well on 12V input and 5V output up to 20A.

Here is the module circuit

Here is the module circuit.

I am trying to add a CV/CC function to limit the output within 0.6-5V, 0-10A.

Here is the new circuit with opamp added.

However, the module get oscillation if opamp output connected to FB pin. How could I solve this problem?

Thank you all.