This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8863-Q1: LP8863 - flickering led

Part Number: LP8863-Q1


LP8863-Q1_Design Tool_for Publish_Final_Protected_10_07_23.xlsxBLC_V1_5942760_PDF_29_08_23.pdf

Hi,

I drive leds with the lp8863.

The power on the card is O.K and the SPI communication working.

The leds are flickering (all the time after I complete the required setup).

I attached the card schematic and the LP8863 design tools with the values I used.

I didn't find setup which could make flickering, so I think it's fault and recovery condition occur in infinite loop.

Pls. review the schematic and advise the needed changes.

Regards

Zeev gerber