Hi TI Teams,
We encountered the following problem when using the bq27220 as a 1-cell LiCo battery to monitor the power level.
1) Gauge drift - multiple charging cycles cause charge percentage value shift from correct to the wrong one.
By gauge drift we mean offset in coulomb counter data, for example gauge reporting 200mah left when battery completely drained. So both battery charge percentage and remaining capacity is incorrect.
2) Shutdown event generated too late - when voltage < 3.2V. We’ve calculated curves with 0.5/1A load and CellTermV 3.3V and it’s clear to us that this was wrong and we need to redo the whole thing.
System description as below:
● 1 cell LiCo battery 3.7V 2100mah with it’s own protection IC (DW01).
● Main board using bq27220yzfr fuel gauge
● Board current consumption: idle ~1ma, active ~300ma, peak 2A
● Target shutdown voltage at 3.2~3.3V
So we have the following question of how to generating the correct profile parameters for bq27220.
1)Which conditions/parameters should we use to generate data for the CEDV calculator?
2) What gauge parameters should we fine tune to get best performance? We’ve been using https://www.ti.com/tool/GPCCEDV to generate parameters for the gauge, and the original parameters and test conditions were not optimal.
Thanks,
Kind Regards