This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373: PSE Negotiation Feedback

Part Number: TPS2373
Other Parts Discussed in Thread: TPS2372

Hello team,


It is unclear if the part can detect the difference between Class 5/6  as well as class 7/8 negotiations with a switch. This is important for the product (ie detection of class 5 vs 6 and class 7 vs 8 for operation).

In Table 2 in the data sheet, it looks like the TPH, TPL and nBT lines are all the same output for Class 5/6 and class 7/8.

Is there any other way with this part to distinguish between the classes? We really only need to know 12.95, 25.5, 40, 51, 62 and 71W allowances.

 

Thanks.