Part Number: UCC2895
Hi,
1. What is the difference between "Frequency" and "Frequency total variation"? Does the frequency total variation mean that the frequency varies further from fosc?
For example, when fosc=500kHz, it varies from 475kHz to 525kHz. When fosc=527kHz, it varies from 500.65kHz to 553.35kHz.
![]()
2. Could you tell me more about why the fosc varies? Is it caused by the comparator or flip-flop shown below?

Best Regards,
Nishie