Hi ti Team,
What is the leakage current when BQ25618E is full?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Someone will get back to you by next Tuesday.
Regards,
Mike Emanuel
Hello,
Please check out:
1. IQ_BAT, or Quiescent battery current (BATSNS, BAT, SYS, SW). This is typ 9.5 uA and max15 uA.
2. ISHIP_BAT, or Shipmode battery current (BATSNS, BAT, SYS, SW). This is typ 7 uA and max 9.5 uA.
Regards,
Mike Emanuel
Hi Michael,
1. IQ_BAT, or Quiescent battery current (BATSNS, BAT, SYS, SW). This is typ 9.5 uA and max15 uA.Is IQ_BAT an Ibat leakage current?
Using EVM tests are as follows:
Ibat leakage when the battery full charged.
Test condition:BAT = 4.35V(Cut-off voltage), VBUS = 5V, SCL, SDA = 0V or 1.8V, BATFET enabled ,Ibat leakage current=110uA
Why is the Ibat leakage current 110uA when Vbus=5V?
Hello,
Please check your pullups. Pullups on I2C, CE, etc. will cause leakage from the battery as well.
Regards,
Mike Emanuel
Hello,
With battery charge voltage limit set to 4.35 V, VBAT voltage at 4.43 V (BATOVP), SDA at 0 V, and VBUS at 5.19 V the leakage from the battery is 105 uA. With the same conditions with VBUS at and above 5.67 V, the leakage from the battery is expected 13.7 uA. With the same conditions with VBUS below 3.35 V, the leakage from the battery is expected 9.7 uA. Please keep VBUS disconnected, above around 5.67 V, or below around 3.35 V to achieve desired IQ.
Regards,
Mike Emanuel
Hello,
We are working to investigate this. Can you please explain your use case and how this affects your solution?
Regards,
Mike Emanuel
Hello,
We are working on updating our datasheet for the next revision. As stated earlier, please keep VBUS disconnected, above around 5.8 V, or below around 3.2 V to achieve desired IQ.
Regards,
Mike Emanuel