Part Number: EV2400
Other Parts Discussed in Thread: BQSTUDIO
Hi experts,
I updated my computer to Windows 11 and I have a problem with communication with the EV2400,
when I open bqstudio I get an error on the bottom "No free adapters are available for use on this system."
when I try to update firmware I get "Error: No Free EV2400s Detected. If one is connected but the LEDs are not on, try running this program with the -s option.
Press enter to continue...".
but if I test it on another computer the update works fine.
I tried different USB ports and nothing helped.