Part Number: BQ25886
HEllo team,
i have some question regarding BQ25886 IC, which are listed below.
1. what is the use of D+ and D- pin of BQ25886?
2. What is OTG mode in this IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
"1. what is the use of D+ and D- pin of BQ25886?" -- Bill J -- Take a look at SLUAA94 Applicaiton note on USB D+ / D-
"2. What is OTG mode in this IC?" -- Bill J -- Take a look at this article on OTG. Also application note SSZY001
Hi
Can I take battery voltage at the "SYS pin" when battery is not in charging mode?
Bill J -- Yes, this will work.
Can you please suggest how to limit the input current?
Set R-ILIM (pin 8) to 370 ohms.