I have designed a buck converter using UC3843 in the following specification,
Vin- 12V to 60V
Vout- 10V
Iout- 200mA
main switch is P type mosfet
The problem is, UC3843 how to driver the P-mosfet in this wide input range..
Please help me to develop a proper design using uc3843 for the above spec.
Regards,
Jack.leung