This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM62435-Q1: Can the BIAS pin be higher than VIN?

Part Number: LM62435-Q1
Other Parts Discussed in Thread: LM25148

Hello,

I want to supply the LM62435's BIAS pin from an external 5 V regulator. However, sometimes this external regulator will be on when the LM62435's VIN is off; i.e VIN=0 V and BIAS=5V. Is this supported?

Another part I plan to use (the LM25148) doesn't allow an external bias greater than VIN, but for the LM62435 it looks like it would be OK based on the datasheet and a quick diode-check with a multimeter. But I'd like to make sure.

Thanks!

Matt