Hello E2E community,
I am currently debugging a design based on the BQ500110-EVM and the BQ51013-EVM.
When I apply power to the BQ500110 and probe the COIL_PWM pin I do see the three 100kHz pulses except they occur every 0.4 sec instead of 0.5 sec (EVM user guide states it should be 0.5 sec). I also notice that sometimes (around 10 - 20% of the time) the BQ500110 will output a 175kHz square wave for about 50 ms instead of the three 100kHz pulses.
Should this be happening? or should I just be seeing the 100kHz pulses until I place my reciever on the transmiting coil? (I dont have an EVM kit to do these tests).
Any feedback or comments would be much appreciated