This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700: Device recommendation inquiry

Guru 11480 points
Part Number: TPS63700
Other Parts Discussed in Thread: TPS65131, LMR43620

Hello,

My customer is looking for a device with the conditions below.

  - VIN = 5V , VOUT = +15V ad -15V , IOUT = 500mA

1. Is there a power device that satisfies the above conditions in one package? please recommend it.

2. If it is not supported by one package, please recommend a product that supports +15V and -15V respectively for 5V input. They prefer products that can be designed into the smallest package area.

3. If there is a product with 15V input and -15V (500mA) output, please recommend it.

Thank you.

JH