This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: Product recommendation

Part Number: TPS61023
Other Parts Discussed in Thread: TPS61299

Hi expert,

my customer want to use TPS61023 to work in this condition(Iomax=2A).  Is TPS61023 suitable in this case or  do we have a better solution? thanks!
(1)4<Vin≤5V, Vo=5.2V
(2)5V<Vin<5.2V, Vo=5.2V
(3)Vin=5.2V,Vo=5.2V
(4)5.2V<Vin<5.5V,Vo=Vin.

And the customer is afraid that when Vin is around 5.2V, Vo will jump between 5.2V or higher volt. they want to make sure that the output is stable.

  • Hi Zoey,

    From your description , I think TPS61299 is more like it.

    TPS61299 will stay in downmode when Vin is around the Vout target, which allows it to work when Vin=Vout.(Boost mode can only regulate when Vin<Vout).

    Best Regards,

    Travis