This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: Iout Current Datasheet Errror?

Part Number: UCC39002

Hi all, 

I was going through the datasheet for the UCC39002 and I noticed an error with units for the output current in the Load Share Driver (LS) section of the datasheet. I suspect that this is meant to be in mA, but could you confirm this for me and update the datasheet if possible?

Thank you.

  • Hello Filipe, 

    Yes, I confirm that the units for the high-lighted row should be mA, not V. 

    Actually, we are already in the process of correcting that datasheet for that error and many many others, including the min/max limits for the LS bus driver "Vout" spec three rows above your high-lighting.  For the condition Vcso = 10 V, the min/max of Vout should be 9.95 and 10.05, not 0.995 and 1.005.

    Regards,
    Ulrich