Other Parts Discussed in Thread: LMR33620, LMR33630, LMR36510, LMR38010
Hi.
What are the criteria applied to the L calculation formula in page.18?
If VIN=12V, VOUT=5V, fSW=400KHZ, K=0.3, and Iomax=1A, the L calculation is 24.3uH. How does L=8.1uH come out?
Even in TABLE9-3, the L value of 5V and 400KHZ is 8.2uH, and the L value of 1400KHZ is 2.2uH.
It is calculated as 24.3uH/6.94uH.
What is Iomax? Is it the max current of lmr33610 or the max current of the circuit load?
BR.
KWON.