Dear Team,
i have some questions regarding TPS6521905 PMIC.
1) if i understand correctly if the PMIC NVM is not programed all BUCK and LDO outputs are off?
1a) if we want to do in-circuit NVM programming once the PMIC is soldered to our PCB , is it possible and what signals do we need to provide from outside to do this?
2) Is it possible to tie the LDO1 and LDO2 output together if they have same output voltage to support 800mA ?
3) if BUCK1 or BUCK2/3 is not used what is the proper way to terminate it from HW and SW side?
4) if LDO3 and LDO4 are not used what is the proper way to terminate it from HW and SW side?
Best Regards,
d.