What is the Max PWM Freq for TPS92611-Q1 using PWM Input pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kmb,
What is the frequency that you want to use? This device has some time requirements. Normally no larger than 2kHz.
1) We have a min PWM-on time requirement, it should be > open/SG fault deglitch time if you want to keep this fault diagnostics.
2) For PWM signals, the t(PWM_delay_rising) and t(PWM_delay_falling) would also affect the PWM on/off time, so it is better to consider the error influence for PWM duty cycle.
BR.
Hailee.