Other Parts Discussed in Thread: TPS55289, , USB2ANY
Hello,
I am currently utilizing the TPS55289 Buck-Boost Converter Evaluation Module, employing the power LED as a load. In my testing, I supplied an input voltage using a DC power supply set to 4.5V/10A. The TPS55289 toggles the LED on and off promptly when the TPS55289 output is set to 5V, and I disabled the current limit through the software available at https://dev.ti.com/gallery/view/TPS55289/TPS55289/ver/1.1.0/.
However, I encountered an issue when setting the TPS55289 output to 4.2V. While the LED functions properly at a current of 4A, my requirement is to drive the LED at 6A. While this can be achieved by directly supplying DC power supply to the LED with 5V, my application necessitates the use of an 18650 battery to drive the LED to 6A.
But if I supplied the TPS55289 with panasonic NCR18650GA, the LED works properly while setting the TPS55289 output to 5V and disable current limit but the LED current is 5A no more even I increase the TPS55289 output more than 5V.
I would appreciate your guidance on this matter.
Best regards,
Sakar