What tolerances should I expect for over/under voltage, over charge, discharge current, ect...?
I couldn't find the answer in the datasheet or TRM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What tolerances should I expect for over/under voltage, over charge, discharge current, ect...?
I couldn't find the answer in the datasheet or TRM.
Hi Aidan,
By tolerance in protection you mean how long the gauge can take to trigger the protection? If so, the gauge can take up to 1 second to trigger Firmware based protections.
Regards,
Jose Couso
Hi Jose,
I meant if the overvoltage protections is set to 4300 mV, is there a range of values that may trigger it +- some percent?
I assume it isn't going to trigger exactly at 4300 mV, so what tolerance does the design need to handle?
Hi Aidan,
See below.
Protection will be triggered based on temperature since the device will adjust charging voltage based on temperature.
Regards,
Jose Couso