This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: BQ25606: please Confirm and review this BQ25606 circuit

Part Number: BQ25606

Hello TEAM.

I use BQ25606 chip, and so i need your help.

my SPEC(6800mAh charging)

1. adaptor(use to 2A), 1.5A charge
1.5A charging to battery(Li-ion)_6800mAh

2. No OTG,No I2C, No D+/D-

3. Use SYSOUT voltage as mcu power source (3V will be applied using DOWN CONVERTOR)

4. Check to battery capacity
-> Check battery voltage using ADC I/O (checkpoint is BAT_3.7V) (left of TP11)

Please look at this circuit below and let me know if you can review it