Other Parts Discussed in Thread: LMR51450, LMR14050
Hi team,
my customer Narwal that EE is robot vacuum cleaner. they use LMR23630ADDAR but it's Output current is 3A which is too small. could you help recommend a pin to pin Buck for them? The requirements as below:
- Input voltage is 11V-18V
- Output voltage is 3.8V-3.95V, accuracy ±5%
- Output current up to 4.5A
- PIN to pin with LMR23630ADDAR
If we don't have pin to pin device. You can also help other more suitable device. Thanks.
Regards,
Amber