This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543B20: TPS543B20RVFT schematics verification (1V35)

Part Number: TPS543B20

Hi,

Please verify the attached schematics and provide feedback.

Vin - 12V, Vout - 1.35V, 50A (2 stacked)

/cfs-file/__key/communityserver-discussions-components-files/196/6355.TPS543B20RVFT_2D00_1V35.pdf

Thanks

  • Hello,

    The schematic looks good from my end.

    One thing to note is that the second regulator has pin 39(RT) populated with a 22.6kohm resistor like in the first regulator. If the first regulator is the master then the second regulator's pin 39 can be left open.

    ,Cesar