This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A45: DC 6V Input

Part Number: TPS7A45

I am looking for an LDO with a ・ 5.5V 1.2A (peak max.) output and I am thinking of using the TPS7A4501DCQ.
Is there any problem even if the input/output voltage difference is 0.5V?