Other Parts Discussed in Thread: BQSTUDIO
Hello,
We are testing a 6S1P pack with nominal 3450mAh capacity. I am trying to understand how the capacity and state of charge readings are generated. See screenshot below:

This was taken during a 2A discharge test after fully charging the pack. First, I should mention that the Full Capacity reading will get up around 2650mAh after charging, but never reaches the 3450mAh programmed into the data registers. So my first question is why can't we get to the full capacity? Second, during this discharge test, the full capacity reading jumped abruptly from ~2600 to ~800mAh, even though cells are still at ~3.7V. What caused this?
Finally, what are the differences between absolute and relative SoC? What are the differences between Full charge and remaining capacity?
Thank you,
Jamie