Hello,
In our design, we use one TPS543C20A and two TPS543B20 to generate three power rails from 12V.
In order to avoid too much current demand on the 12V, we apply on each converter a external signal on the sync pin (each signal is phase shifted by 120° from the others to make the converters drawing current alternaltively).
These 3 signals are generated by a microcontroller. The issue we have is the following : while reprogramming the microcontroller, the sync signals aren't generated anymore during a few seconds. Then, the SYNC pins of the converters do not receive the signal anymore, which make the power rails going down. We expected the converters to toggle on its internal pulse generator (frequency set by RT pin) when loss of signal on SYNC pin occurs, but it seems this is not the case.
Is that a normal behaviour ? Is there way to keep this synchronization feature and having ability to keep power-on state even if synchronization signal is lost ?
The converter is set is standalone mode, with API/BB off (MODE = open). We have verified that the frequency set by RT pin is below the frequency of external sync clock.
See schematic extract for one of the power rails (+12V to +5V) : https://ibb.co/1dfBnjd
Thanks.
Alexandre