Part Number: BQ40Z50
Hi
I am trying to observe an RA table update by monitoring the RX bit in the Gauging Status register while discharging the battery, the RDIS bit is set constantly so I cant observe the update.
The update status register is 0x0E
I noticed when using BQ studio gas gauging is enabled by default ( I presume BQ studio sends a command to enable it on startup as the TRM says gas gauging should be disabled), if I disable gas gauging wait a second and then re enable gas gauging again the RDIS bit will clear.
This creates some uncertainty as I am now not sure if the RDIS bit is set due to incorrect gauge enabling or for another genuine reason.
Regards
Ian