Hello,
I have implemented the TPS25970ARPW for over current protection at 1.3A. The device goes into current limiting mode when the quiescent current is between 1.28 and 1.32A; however, if the load draws above this current value the device latches off and does not recover until a power cycle is performed. This is unexpected as the device appears to be in the Auto-Retry mode until a certain point where it latches off and shuts down. I have attached the device schematic for reference.
Any suggestions or comments on why this is happening would be appreciated. Thanks