This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5012: 5V to VCC pin ok

Part Number: LP5012

Hello

I just want to confirm this is acceptable and correct:

Going to use LP5012 in a design where the I2C is shared between different slaves ( addr. is different ), the pull up resistors for SCL and SDA is connected to 3.3V.

LP5012 will be driven by +5V at VCC pin.

The EN pin will be driven by the +3.3V logic, EN pin is only input.

Since LP5012 have an internal LDO it is ok to drive it this way.

Thank you for your help!