What is the best value of output capacitance to keep the output impedance of the REF35 low through 10 Khz ? By low I mean 100 ohms or less through 10 khz ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the best value of output capacitance to keep the output impedance of the REF35 low through 10 Khz ? By low I mean 100 ohms or less through 10 khz ?
Hello,
The REF35 datasheet includes Figure 7-26 which shows the output impedance for output capacitor loads 0.1 µF, 1 µF, and 10 µF:
The stable output capacitance range is 0.1 µF to 10 µF. I would expect values in that range to be around what is represented in Figure 7-26. I would recommend selecting an output capacitance in that range.
What is your application circuit that is causing the need for such a low output impedance? Is a buffer something you could consider to meet this output impedance spec?
Thanks,
Jackson