Hello guys,
One of my customers is considering using TPS922055 for their new products.
At this moment, they have the following question.
Could you please give me your reply?
Q.
The following FAQ says that TPS922055 operates with CC (Constant Current) mode when UVP voltage is more than 1.4V.
Also the device datasheet says that the device stops switching when UVP is less than 1.0V.
The customer wants to know what TPS922055 operation is when UVP is between 1.0V and 1.4V.
Is it hysteresis for LED open detection? So TPS922055 stops switching when the OVP terminal voltage goes less than 1.0V and goes back CC mode operation when the OVP terminal voltage goes higher than 1.4V?
Your reply would be much appreciated.
Best regards,
Kazuya.