Part Number: UC2844
Hello,
My customer is testing the UC2844N on a board they designed with the conditions below.
- specification : 220VAC±20% Input, 28V/3A output, Effi 85%
- Switching frequency : 70kHz
- Topology : Flyback
- Control IC : UC2844N
- Transformer :`

Error symptom 1 : Burst mode operation when load is applied - actual output falls in the burst section and rises in the pause section

Ch1. Vgs, Ch2. Vo, Ch3. Isense, Ch4. Vds
Error symptom 2 : Isense noise occurs when FET switching ON/OFF - Isense noise -> Output noise

Ch1. Vgs, Ch3. Isense, Ch4. Vds
Q1. Please advise on the causes and solutions for the above error symptoms.
Q2. Could you please review the circuit privately to see if there are any problems?
Thank you.
JH