This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: LM5117 Spice Error in Microcap-12

Part Number: LM5117


I am trying to simulate SNVA829 (constant current constant voltage) schematic given in the application report from TI. I downloaded the spice model from TI site and imported it to microcap. When I tried to run the transient analysis I get the following error (seems it's a warning but it doesn't start or complete the simulation due to the warning); Warning: Extra Text 'TC=0,0' found. Part: X4.C_C1 File:.......... I want to get the simulation working since I want to change the design so that it works for my application. Is there an issue with the model provided by TI? I downloaded the zip folder snvm960 and used that model since that's the only unencrypted model I could find