This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060: Please help to review the circuit diagram

Part Number: TPS43060


TPS43060RTET 24V TO 53VTPS43060RTET 24V TO 53V (1).pdf
Boost应用, INPUT 24V,OUTPUT 53V@2A
 
Please help to review the circuit diagram
  • Hello Winnie,
    Thanks for reaching out to us via e2e.

    The schematic looks fundamentally o.k. But I did not yet have time to look at every component.

    Can you please specify the input voltage range?
    For lower input voltages the inductor might run into saturation.

    How did you calculate the external components?
    Have you used the Quickstart Calculator which you can find here:
    www.ti.com/.../SLVC471 ?

    You can send us the filled-in Excel sheet and then we can have a look at it.

    Thanks and regards,
    Harry