This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25157: BQ25157 ADCIN with external NTC

Part Number: BQ25157

Hi, 

I would like to connect an external 10k ohm NTC to the ADCIN pin.

should I connect it directly to the pin or use additinal parallel resistor (Rp=10K ohm) like the way the NTC connected to the TS pin?

Thanks,

Uri