Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515-Q1: Maximum switching frequency

Part Number: TPS92515-Q1
Other Parts Discussed in Thread: TPS92515HV

What is the maximum switching frequency of the TPS92515HV?  Assuming maximum output current of 2A.

  • It is actually affected by many factors in the design, such as input, output voltage range, power loss, operation temperature etc. 

    For example, frequency variants with output voltage and/or input voltage. Thus, highest frequency happens @ Vin= Vin,max, Vo=Vin/2;  

      

    Also, you need to consider power loss in device and acceptable junction temperature rising under worst condition. For power loss and junction temperature, you may refer to 8.3.9 Junction Temperature Relative Estimation in datasheet. Make sure that efficiency and thermal dissipation is ok with highest frequency.