Other Parts Discussed in Thread: LM5143, LM5148, LM5143-Q1
Hi wish to know , about Q current during interleaved single-output
We are using LM5143-Q for the 40A Max Operation & 25A continuous Operation with input upto 36V Max & output upto 14.2V
We are using two phases interleaved , during such interleaved condition we have to connect MODE pin to GND right?
Now during such condition what would be Q current ? , also let us know about the what can we do to reduce Q current
Regards,
Anish Salvi