Hello.
We are conducting an experiment on an ORing circuit using the evaluation board TPS23525EVM-815.
With a constant voltage of -40V applied to the A input, we have gradually increased the voltage on the B input to see if there is any through current from the A input to the B input or from the B input to the A input at the switching point.
When the voltage of the B input is changed slowly, no through-current flows, .

but when it is changed quickly, it appears that a transient through-current flows momentarily

Q1 Please explain how the prevention mechanism inside the TPS23525 works to prevent through-current from flowing from the A input to the B input or from the B input to the A input.
Q2 Please explain why a transient feed-through current flows when there is a quick switchover, and how the prevention mechanism mentioned in Q1 works in this case.