This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL7660: application problem.

Part Number: TL7660


hi team,

customer intended to use the TL7660 to design a circuit that turns a positive (0, 5V) signal into a negative (-5V, 0V) level, but the actual test did not meet expectations, the actual situation as shown in the oscilloscope diagram, is the output level jumps when the input signal goes down. how to achieve the positive level control output negative level function.